AXIS#.GEAR.DEC
Description
AXIS#GEAR.DEC defines the maximum deceleration rate the slave follows to come out of gearing, to rest. AXIS#GEAR.DEC is only be used if Gearing is stopped for any reason, including if an AXIS#.STOP command is issued. When the axis comes to rest, AXIS#GEAR.DEC is no longer in effect and the axis behaves according to the rules of the motion commanded next.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2 See Acceleration Units for details. |
|
Range |
Depends on units. See Acceleration Range for details. |
|
Default Value |
10,000 RPM/s Depends on units. See Acceleration Units for details. |
|
Data Type |
Float |
|
Stored in Non-Volatile Memory |
Yes |
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.GEAR.DEC |
5006h |
02h |
Unsigned32 |
Acceleration |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5501 |
1 |
5501 (0x157d) |
AXIS1.GEAR.DEC |
Unsigned32 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.GEAR.DEC |
5501 |
Float |
Read/Write |
Acceleration |
Variants Supported
All variants are supported